While discussions surrounding AI infrastructure traditionally focus on compute performance, the conversations at Yotta 2026 added new layers to this narrative: cooling, power, and deployment speed are quickly becoming the factors that determine whether AI capacity can actually scale.
Yotta 2026 brought together leaders from across the AI infrastructure ecosystem to discuss one of the industry’s biggest challenges: how to scale the cooling, power, and physical infrastructure needed to support the next generation of AI workloads.
As part of Schneider Electric’s presence at the event, Motivair experts were onsite to discuss the growing role of advanced liquid cooling technology in data center infrastructure. Attendees had the opportunity to connect directly with the Motivair team to explore the strategy behind scalable cooling infrastructure, deployment efficiency, operational reliability, and supporting high-density computing environments.
Visitors to the Schneider Electric booth explored how integrated cooling, power, and infrastructure strategies can help organizations successfully keep up with the ever-evolving demands of high-performance computing.
AI rack densities continue to rise. Organizations are preparing for increasingly power-dense environments that require new cooling architectures.
Deployment speed is becoming a competitive advantage. Infrastructure teams are focused not only on capacity, but also on how quickly AI-ready environments can be deployed and scaled.
Cooling strategy is becoming paramount earlier in the planning process. As AI workloads grow, every increase in compute requires corresponding investments in thermal management infrastructure.
Coolant distribution units (CDUs)
Motivair’s CDU portfolio spans multiple models that come with cooling capacity up to 3.5MW. And with redundancy and reliability built into the architecture of each floor-mount and in-rack CDU, IT infrastructure will remain operational even under extreme thermal and computational loads.
ChilledDoor®
The ChilledDoor rear door heat exchanger can support rack densities up to 75kW and seamlessly integrates into any industry-standard server rack. Made for high-performance computing environments, the ChilledDoor removes 100% of heat right at the rack level, enabling peak performance.
Missed Motivair by Schneider Electric at Yotta?
With support from Schneider Electric, Motivair will be present and ready to connect with customers at SC26 in Chicago from November 16–19. Find the Motivair team of experts at Booth 3823 with innovative products from their end-to-end liquid cooling portfolio including the CDU-50, ChilledDoor, and HDU™.