Motivair Cool News

November 16th, 2026

Cooling AMD Helios: The New Dual ChilledDoor®

Motivair by Schneider Electric is introducing a new dual ChilledDoor® rear-door heat exchanger purpose-built for the AMD Helios™ rack-scale platform, coming to SC26 this November.

As AI workloads become larger and more complex, the systems built to run them are evolving as well. AMD Helios™ represents that shift toward full rack-scale AI, bringing GPU, CPU, networking and software together into an integrated platform designed for high-performance AI workloads.

Powered by AMD Instinct™ MI455X GPUs, 6th Gen AMD EPYC™ CPUs, AMD Pensando™ Vulcano NICs and the open ROCm™ software ecosystem, Helios is designed to enable larger, more complex AI workloads while optimizing power and efficiency.

That shift has implications beyond compute. The double-wide Helios rack introduces a different physical architecture, and the cooling infrastructure supporting it has to adapt.

A new rack architecture creates a new cooling challenge
In July, Schneider Electric and AMD announced a jointly developed and validated reference design for Helios designed to support AI racks up to 246 kW and modular AI clusters of up to 10.4 MW of IT capacity. The architecture brings together power, cooling, IT space and lifecycle software to provide a blueprint for deploying high-density AI environments.
At these densities, cooling is not only a capacity question. It also has to account for the physical configuration and thermal requirements of the rack itself.

That is the thinking behind the newest ChilledDoor® from Motivair by Schneider Electric.

Purpose-built for AMD Helios™
Rather than adapting a conventional ChilledDoor® to a new rack configuration, Motivair by Schneider Electric engineered a dual-door design around the AMD Helios™ platform.
The dual ChilledDoor® provides up to 75 kW of room-neutral cooling, capturing heat directly at the rack and minimizing heat rejected into the surrounding data center environment.

For operators, that means a cooling solution aligned to the physical configuration of the Helios platform, designed to capture heat at the rack and scale from individual systems to larger deployments.

Part of a broader cooling architecture
The Schneider Electric and AMD Helios reference design incorporates Motivair by Schneider Electric CDU-based liquid cooling and hybrid air/liquid approaches alongside the power and digital infrastructure required to support high-density AI environments.

The new dual ChilledDoor® extends that approach directly to the Helios rack architecture.

Rather than treating direct liquid cooling and room-neutral rear-door cooling as separate strategies, the architecture brings cooling technologies together around the requirements of the compute.

Designed to scale with AI
The dual ChilledDoor® system is designed to scale from a single Helios rack to larger AI deployments, providing a repeatable approach to heat capture as infrastructure expands.
That rack-level scalability complements the broader Schneider Electric and AMD reference design, which supports modular AI clusters up to 10.4 MW of IT capacity.

See it at SC26
The move to rack-scale AI isn't simply changing how compute is packaged. It is changing the infrastructure required to support it.

At SC26 this November, Motivair by Schneider Electric will showcase its new dual ChilledDoor® technology for AMD Helios™ at booth 3823, demonstrating a cooling solution engineered specifically for the next generation of rack-scale AI.

Connect with your local Motivair product specialist today.

TOP