Motivair Cool News

May 19th, 2025

Unlock NVIDIA’s AI‑Factory Vision: Discover the Liquid‑Cooling Advantage

NVIDIA CEO Jensen Huang’s latest COMPUTEX keynote recasts data centers as AI factories — industrial scale engines that turn energy into high value “tokens” powering every sector of the economy. Below is a concise tour of the announcements and the thermal realities behind them.

  1. AI Infrastructure Becomes a Trillion Dollar Market
    Huang compared AI infrastructure to electricity and the internet, predicting an era in which national and corporate AI factories become foundational utilities. The growth curve is steep, and so is the heat load.
  2. NVLink Fusion Opens Semi Custom Scale
    The new NVLink Fusion architecture lets hyperscalers mix CPUs, GPUs and custom accelerators across a common fabric, breaking traditional bottlenecks and driving unprecedented rack densities.
  3. Blackwell Everywhere, DGX Spark on Every Desk
    “Blackwell” now spans cloud to edge, while DGX Spark personal supercomputers and RTX PRO servers democratize multi petaflop performance. Expect AI workstations on desktops and multi megawatt clusters in the same enterprise.
  4. Digital Twin Pipelines for Physical & Agentic AI
    Omniverse powered blueprints are scaling from chip plants to humanoid robot training grounds, turning simulation into an everyday engineering tool. But digital twins only deliver value when the physical hardware can sustain peak performance, 24/7.

WATCH NOW: Jensen's Computex Keynote here. | LEARN MORE: See our ChilledDoor® featured in AIST’s ABCI-Q Supercomputer

Liquid Cooling: Turning Vision into Reality

Massive computational density demands equally advanced thermals. Motivair by Schneider Electric provides a portfolio purpose built for NVIDIA class workloads:

  • The Widest Range of Coolant Distribution Units (CDUs)
    Trusted by leading data centers and HPC facilities, Motivair CDUs cool up to 2.3 MW. Designed in collaboration with top silicon manufacturers — including NVIDIA — they integrate seamlessly with next gen processors and accelerators, safeguarding uptime and efficiency.
  • Motivair’s ChilledDoor® Rear Door Heat Exchanger
    Engineered for racks up to 75 kW, ChilledDoor® tames thermal peaks from GPUs such as the NVIDIA H100 series. Its rack agnostic design slots into existing or new deployments without structural changes.
  • Liquid to Air Heat Dissipation Unit (HDU™)
    HDU bridges liquid-cooled hardware and air-cooled facilities, perfect for AI accelerator boxes, colocation sites, or lab environments where facility water isn’t available.
Ready to Build Your AI Factory?

Whether you’re scaling a single DGX Spark lab or a multi megawatt Blackwell cluster, Motivair’s liquid cooling ecosystem delivers the thermal headroom to keep innovation moving. Let’s chart your path from data center to AI factory—without breaking a sweat.


Connect with your local Motivair product specialist today.

TOP