Air-cooling technology, which has defined the cooling landscape from early computer rooms to today’s data centers, is giving way to a new era. Air-cooling alone is no longer enough to keep up with increasing workloads and rising AI demands. The industry is facing a paradigm shift, one that requires more than incremental fixes.
For more than 50 years, computer rooms and data centers relied on CRAC (Computer Room Air Conditioners) or CRAH (Computer Room Air Handlers). These systems sat outside the racks in the data hall, blowing chilled air into the room while server fans pushed it across components.
Air cooling worked well in its time, typically supporting ~15–20 kW per rack. But today’s rapid AI evolution and HPC workloads push far beyond those limits, with modern racks regularly exceeding 70–100 kW.
During this era, IT teams focused on servers and storage while facilities teams oversaw HVAC and power. These groups often worked in silos - connected loosely but rarely collaborating on cooling strategy. The result was efficiency, but not optimization.
Liquid cooling isn’t new - it’s been used in transformers, mainframes, and supercomputers for decades. What’s different now is the density of AI and HPC systems, which generate heat loads that air cooling simply cannot manage.
Liquid cooling increases processing power and efficiency while reducing operating costs. More importantly, it enables rack densities and performance levels that are otherwise impossible.
In this era, cooling moves inside the racks with solutions like cold plates, CDUs, and in-rack manifolds tied directly to plant-room supply. Success depends on water chemistry, flow stability, and filtration (often down to 25 microns).
When these converge, operators achieve thermal stability, reduced downtime risk, and scalable efficiency.
Many providers oversimplify, offering part of the solution. Catalog vendors may sell individual SKUs, but they cannot deliver a holistic cooling architecture. Motivair takes a different approach.
We own the full thermal chain - from fluid dynamics and manifold design to cold plate strategy, control, sensing, and facility integration. This ensures IT and facilities are no longer loosely connected but instead work together under a single, unified strategy.
What does this mean for customers?
With decades of advanced cooling expertise, Motivair delivers direct liquid cooling systems built to handle AI and HPC workloads - while preparing data centers for what comes next.
At Motivair, we do more than make cooling work. We create the bridge between IT architects and facility engineers, transforming cooling from a background utility into a strategic enabler of AI.