Motivair Cool News

April 20th, 2023

Motivair to Exhibit at ISC High Performance 2023 in Hamburg

Motivair Corporation, a global leader and innovator in cooling digital infrastructure, will showcase its portfolio of direct liquid cooling technology May 21-25 at ISC High Performance 2023, an international conference and exhibition that fosters the growth of a global HPC community of technology providers and users.

Attendees can also visit booth A104 to see examples of its Coolant Distribution Units (CDUs), the ChilledDoor® rack cooling system, and a comprehensive End-to-End Liquid Cooling Portfolio designed exclusively for HPC, AI and Big Data users.

Dynamic™ Cold Plates: Scalable and patented technology that delivers thermal performance to +1,000 watts per processor for leading CPUs, GPUs, APUs, and FPGAs.

  • Thermally targeted cold plate technology that’s unique for each processor SKU
  • Scalable performance designed to enable multiple product generation roadmaps
  • Available for the following processors: AMD SP5 Genoa and SP3 Milan, Intel Sapphire Rapids and Ice Lake, and NVIDIA SXM4, and customer-specified FPGAs, or custom silicon.

The Widest Range of CDUs: Cool up to 2.3MW with Motivair’s portfolio of CDUs. Motivair’s CDUs represent the widest range and highest capacity of standard and custom OEM CDUs available.

Motivair’s ChilledDoor®: Server and rack agnostic active rear door heat exchanger that cools rack densities up to 75 kW per rack. Ideal for air-cooled, high-wattage processors like intel ice lake and sapphire rapids.

End-to-End Cooling Portfolio: Motivair’s End-to-End Liquid Cooling product portfolio allows systems to be optimized for reliability and performance. System components include Dynamic™ Cold Plates, Cooling Loops, Hose Kits, In-rack Manifolds, Coolant Distribution Units (CDUs), Heat Dissipation Units (HDUs™) and ChilledDoors® designed and manufactured in the USA for the world’s most advanced HPC, AI and Exascale class systems.

About Motivair Corporation
Motivair enables industry leaders to push the boundaries of what’s possible by leveraging over 30 years of insights and innovations creating dependable mission critical cooling systems. Based in Buffalo, NY, Motivair creates, develops, and manufactures high-density computer cooling systems and a portfolio of specialty chillers that cool vital industries and propel the world’s most complex and advanced technologies. Its technologies are featured in numerous Top500 supercomputers around the globe. For more information, visit www.MotivairCorp.com


Connect with your local Motivair product specialist today.

TOP