Motivair Corporation, a global leader and innovator in cooling digital infrastructure and mission critical applications, will exhibit at the 2024 AHR Expo at Booth #N2756.
The event, Jan. 22-24 in Chicago, Illinois, is the world’s largest HVACR show attracting over 100,000 attendees who are interested is seeing the industry’s latest products, technologies, and ideas.
Stop at booth # N2756 to learn how Motivair is delivering reliable cooling technology that enables the world to solve complex thermal challenges and advances in technology, business, and science.
Attendees can also visit the Motivair booth to see displays its End-to-End Liquid Cooling Portfolio designed exclusively for HPC, Artificial intelligence, and Big Data users, including its mission-critical chillers, Coolant Distribution Units (CDUs), the ChilledDoor®, and Liquid-to-Air Heat Dissipation Unit (HDU™).
Mission Critical Chillers: Specialty chillers designed to accommodate a wide range of operating points, specs, and requirements set by the customer and not a catalog.
The Widest Range of CDUs: Featured in all three USA Exascale Systems, Motivair’s CDUs cool up to 2.3MW. Motivair’s CDUs are designed to enable the latest advances in AI from NVIDA and AMD processors. Made in the USA.
Motivair’s ChilledDoor®: Server and rack agnostic active rear-door heat exchanger that cools rack densities up to 75 kW. Ideal for air-cooled, high-wattage processors like NVIDIA’s H100, Intel’s Ice Lake and Sapphire Rapids. Made in the USA.
Liquid-to-Air Heat Dissipation Unit (HDU™): The HDU enables liquid-cooled hardware such as NVIDIA GPUs in a traditional air-cooled data center environment where water is unavailable. Ideal for use with AI accelerator boxes, colocation, hyperscale datacenters, and labs. Made in the USA.
ABOUT MOTIVAIR
Motivair designs, engineers, and services liquid cooling and data center cooling infrastructure, enabling advanced technologies for tomorrow. It supports the progressive needs of customers, ranging from cooling artificial intelligence and edge computing to colocation and hyperscale data centers, as well as mission-critical applications. Motivair's technologies are utilized by leading silicon manufacturers, server OEMs, and data centers, and are featured in countless Top500 supercomputers worldwide.