Nov. 3, 2023 – Motivair Corporation, the global leader and innovator in cooling digital infrastructure, will showcase its portfolio of liquid cooling technology at SC23, the international conference for high-performance computing, networking, storage, and analysis, in Denver, Colorado Nov. 13-16.
Attendees can also visit booth #1909 to see displays its End-to-End Liquid Cooling Portfolio designed exclusively for HPC, Artificial intelligence, and Big Data users, including its Coolant Distribution Units (CDUs), the ChilledDoor®, Dynamic® Cold Plates, and Liquid-to-Air Heat Dissipation Unit (HDU™).
The Widest Range of CDUs: Featured in all three USA Exascale Systems, Motivair’s CDUs cool up to 2.3MW. Motivair’s CDUs are designed to enable the latest advances in AI from NVIDA and AMD processors. Made in the USA.
Motivair’s ChilledDoor®: Server and rack agnostic active rear-door heat exchanger that cools rack densities up to 75 kW. Ideal for air-cooled, high-wattage processors like NVIDIA’s H100, Intel’s Ice Lake and Sapphire Rapids. Made in the USA.
Dynamic® Cold Plates: Scalable technology that delivers thermal performance up to +1,500 watts per processor. The patented technology allows CPUs, GPUs, and APUs to operate at peak performance. Made in USA.
Available for the following processors: AMD SP5 Genoa and SP3 Milan, Intel Sapphire Rapids and Ice Lake, and NVIDIA H100, and customer-specified FPGAs, or custom silicon.
Liquid-to-Air Heat Dissipation Unit (HDU™): The HDU enables liquid-cooled hardware such as NVIDIA GPUs in a traditional air-cooled data center environment where water is unavailable. Ideal for use with AI accelerator boxes, colocation, hyperscale datacenters, and labs. Made in the USA.
Motivair’s cooling technology is integral with data-driven essentials, mission-critical processes, & groundbreaking innovations shaping tomorrow and accelerating business outcomes. For more information on Motivair, visit motivaircorp.com.
ABOUT MOTIVAIR
Motivair designs, engineers, and services liquid cooling and data center cooling infrastructure, enabling advanced technologies for tomorrow. It supports the progressive needs of customers, ranging from cooling artificial intelligence and edge computing to colocation and hyperscale data centers, as well as mission-critical applications. Motivair's technologies are utilized by leading silicon manufacturers, server OEMs, and data centers, and are featured in countless Top500 supercomputers worldwide.