BUFFALO, NY – Motivair Corporation, a global leader and innovator in IT and Electronics Cooling, announces the availability of its In-Rack Heat Dissipation Unit™ (HDU). The latest model, which officially launches at SC21 in St. Louis (Booth #2601), is an in-rack alternative to its full line of HDUs for adapting air-cooled data centers to liquid cooling.
Motivair’s In-Rack HDU delivers mission-critical liquid cooling where facility water is not available. It comes in two models: MHDU 10 and MHDU 15, with cooling capacities up to 10 kW and 15 kW respectively.
Unlike a Coolant Distribution Unit (CDU) that rejects heat from the server rack to the chilled water loop of the building, a Heat Dissipation Unit (HDU) rejects the server heat from the server rack to the white space where building air conditioning would then remove that heat.
This in-rack unit circulates fluid to direct liquid-cooled cold plate technology, cooling designated chips and rejecting removed heat to the surrounding air. With N+1 redundancy on all critical components and hot-swappable fans, it is designed to operate in a production data center environment.
In addition, the HDU 10 or 15 models may be used in a laboratory environment with an optional bypass attachment that allows for controlled flow down to 1 lpm. Its compact footprint and caster mounted design allow you to move it to selected test stand areas as needed.
Motivair’s Floor Mount HDU cools capacities up to 144 kW.
For more information on Motivair’s Data Center and IT Cooling technology, click here.
About Motivair Corporation
Motivair enables industry leaders to push the boundaries of what’s possible by leveraging over 30 years of insights and innovations creating dependable mission critical cooling systems. Based in Buffalo, NY, Motivair creates, develops, and manufactures a portfolio of specialty chillers and high-density computer cooling systems that cool vital industries and propel the world’s most complex and advanced technologies. Its technology is featured in numerous Top500 supercomputers. For more information, visit www.MotivairCorp.com.