Server rack densities have grown considerably, well beyond the capacity of what traditional air-cooling methods were designed to support. This growth signifies a new phase in the evolution of data center design. Environments that once thrived with air-cooling solutions eventually moved toward hybrid solutions that combined the elements of both air and liquid cooling. And now, the demands of AI have caused liquid cooling to become a non-negotiable element of data center infrastructure.
Instead of planning for eventual liquid cooling adoption, high-performance computing environments are being designed with a liquid-first approach. Meaning, new operations are built under the assumption that liquid cooling will be a necessity in supporting the facility’s lifecycle.
This new phase of data center design represents the elevated importance of thermal management. Thermal management is no longer just a consideration made to support the center’s operational function; it plays a strategic role in the success of that center.
Historically, cooling systems were viewed primarily as support infrastructure, responsible for maintaining uptime and protecting equipment. They removed heat while keeping servers online. The compute an operation could support was determined by factors like available power. And while cooling was important, it wasn’t a driving force behind the planning of a data center’s infrastructure.
The rapid growth of AI has completely changed this narrative. In today’s data center operations, cooling infrastructure has more of a hand in the operation’s server capacity, scalability, time to deployment, and its operational efficiency than ever before. Even when adequate power exists in a data center, if the heat being produced by servers can’t be removed efficiently, the operation cannot reach peak performance.
As AI continues to scale, data center operators have begun to think about thermal management just as they would have once thought about power capacity planning. The ability to manage heat is now key to how much compute can be supported within a facility.
With liquid cooling becoming a more necessary element of data center infrastructure, these facilities need thermal management solutions designed with AI growth in mind. Motivair by Schneider Electric's coolant distribution units (CDUs), heat rejection technologies, and integrated thermal management solutions enable operators to expand their cooling capacity, increase server rack densities, and prepare for the next generation of AI hardware without rethinking their entire thermal management strategy.
One of the most important elements of this new phase of data center infrastructure is the shift from liquid-ready to liquid-first design considerations. While these phrases sound interchangeable, the two represent fundamentally different approaches to infrastructure planning.
A liquid-ready facility is designed under the pretense that liquid cooling solutions may eventually be deployed in the operation. Its infrastructure is planned to primarily support air-cooling solutions and can support the gradual deployment of liquid cooling systems. As AI workloads scale to be even larger, data center operators can retrofit certain liquid cooling technology as thermal demands increase.
On the other hand, a liquid-first facility is designed with the infrastructure necessary for day-one liquid cooling deployment. Thermal management has played a key role in the strategy behind the facility’s design, including considerations made for future expansion. These facilities can adapt simply when AI scales and can handle future generations of high-density compute.
Many high-performance computing environments have started to invest in becoming liquid-ready. But the reality is that a data center simply being capable of supporting liquid cooling isn’t the same as having liquid cooling deployment sewn into its fabric. As AI technology becomes more powerful and produces more heat as a result, it is important that thermal infrastructure becomes a core strategy in data center planning rather than a secondary design element.
The transition from liquid-ready to liquid-first infrastructure requires technology that simplifies liquid cooling deployment and supports future expansion. The Motivair portfolio helps data center operators establish the liquid cooling foundations capable of supporting both current and future generations of high-density compute without requiring structural redesigns.
The data centers being built today will certainly outlive the servers that they initially deploy. In fact, the goal is that these operations will last through a technology cycle that brings about greater performance, higher power consumption, and increased thermal demands without needing costly upgrades to their infrastructure.
This creates a unique challenge for data center operators. Facilities can’t only be designed to meet the needs of today’s AI infrastructure; they must be designed to support hardware upgrades and maintain peak productivity. It is a far greater risk for operators to think only of the present AI moment than it is to consider how an operation will function in the coming years.
Motivair understands that the facilities designed for the future thermal demands of AI are the ones best positioned for long-term success. That’s why the Motivair product portfolio offers scalable liquid cooling solutions that can keep up with the evolving thermal demands of AI.
Along with this shift to a new phase in cooling infrastructure comes a shift in the design philosophy behind high-performance computing environments. Airflow management was once the primary focus of data center design, but the demands of AI technology have changed this focus.
Moving air through a data center becomes a secondary priority when the real challenge at hand is moving heat from the facility as efficiently as possible. This requires data center operators to focus on the thermal architecture of their operation, from the facility water supply right down to the heat generated by the chips in their servers. And as AI workloads continue to scale, thermal architecture continues to prove itself to be a cornerstone in infrastructural design.
Liquid cooling solutions offer significant advantages to these data centers because liquid can transport heat more efficiently than air and allow for higher density environments while reducing the physical limitations associated with air cooling solutions. Because of this, there is now a greater emphasis on those liquid cooling products that prioritize coolant distribution, thermal transport, and system-wide efficiency.
Operations that align with this focus on heat removal rather than airflow management and integrate liquid cooling solutions into the design of their infrastructure will be better positioned to deploy higher-density compute, improve efficiency, and accelerate future expansion.
As the high-performance computing industry moves toward liquid-first infrastructure, the operations best positioned for long-term AI success will be those that treat thermal management as a strategic design decision rather than a deployment afterthought. Motivair by Schneider Electric is here to enable data center operators to design and deploy advanced liquid cooling solutions that support reliable, efficient, and scalable AI infrastructure both today and well into the future.