Motivair Cool News

August 14th, 2024

How to Leverage Air Cooling for NVIDIA AI GPUs

In the world of AI and high-performance computing, air cooling for NVIDIA GPUs is critical to maintaining efficiency and reliability. NVIDIA’s H100 and H200 GPUs offer high power and performance but also generate significant heat. Options to manage the heat include air cooling, a perfect match for Motivair by Schneider Electric’s innovative ChilledDoor® Rack Cooling System.

Unlocking Air Cooling Potential for High-Density GPU Clusters

NVIDIA’s H100 and H200 700-watt GPUs are designed to handle demanding AI and data processing tasks, generating significant heat in the process. While data center liquid cooling is emerging as the option of choice for these solutions, air cooling for GPUs makes sense in many setups.

Motivair’s ChilledDoor® provides effective AI server cooling to keep high-performance processors operating at optimal temperatures. The ChilledDoor® system improves GPU thermal management by stabilizing rack temperature even under peak AI workloads, thereby improving data center efficiency.

How to Optimize Air Cooling for NVIDIA AI Servers

To optimize air cooling for NVIDIA GPUs, it’s necessary to focus on inlet temperatures, not the average data-hall temperature. Monitoring inlet temperature helps prevent localized hot spots that trigger GPU throttling or fan saturation.

Maintaining a clean, predictable front-to-back airflow is important because that’s how GPU servers are engineered. Cabling congestion, missing blanking panels, and open rack gaps create recirculation paths that let hot air reenter the inlet. Sealing these paths solves the problem.

Another issue can arise from exceeding the practical rack power limits for air cooling. Air cooling becomes inefficient and sensitive to airflow imbalance at 25 to 30 kW per rack. If NVIDIA AI deployments exceed this range, operators should either distribute loads across more racks or implement hybrid or liquid-assisted cooling systems.

Best Airflow Design for GPU Clusters

To ensure the best airflow design for GPU clusters, operators should follow these steps:

  • Enforce hot and cold aisle containment. Separating hot and cold air prevents thermal short-circuiting and stabilizes inlet temperatures across GPU rows. Containment is often the single biggest airflow improvement for existing deployments.
  • Eliminate bypass airflow and pressure loss. Raised-floor tile placement, blanking panels, and sealed cable cutouts ensure that cooling air passes through servers rather than escaping into unused spaces. Poor pressure management wastes cooling capacity and creates unpredictable hot spots.
  • Design for uniform airflow, not peak airflow. GPU clusters suffer when airflow distribution varies between racks. Consistent inlet temperature and uniform airflow improve thermal stability, reduce fan energy, and improve system reliability at scale.

The ChilledDoor® Advantage in Air Cooling

Motivair's ChilledDoor® Rack Cooling System improves GPU thermal management by stabilizing rack temperature even under peak AI workloads. As such, it delivers an ideal AI server cooling option for data centers utilizing NVIDIA’s H100 and H200 GPUs. Here’s how it works:

  1. Air Cooling Efficiency: The ChilledDoor® is an active rear-door heat exchanger that uses cool facility water circulated through the system. Fans pull room air through the server racks, where the ChilledDoor® absorbs and transfers the heat to the chilled water system. This process ensures only cool air is exhausted back into the room, providing a room-neutral GPU thermal management solution that removes 100% of the heat generated by the servers.
  2. Scalable and Flexible: The ChilledDoor® system is designed to fit any industry-standard server rack, making it a scalable solution for data centers of all sizes. Its ability to efficiently cool up to 75 kW per rack supports even the most demanding AI workloads.
    Supporting next-generation data centers

Supporting Next-Generation Data Centers

As data centers evolve to support the growing demands of AI and high-performance computing, operators are weighing the benefits of air vs liquid cooling for NVIDIA GPUs for effective GPU thermal management.

By offering effective air cooling for NVIDIA’s H100 and H200 GPUs, the ChilledDoor® system enhances the performance and reliability of these powerful processors, ensuring that data centers can meet the challenges of today and tomorrow.

Get practical guidance on choosing between air and liquid cooling in data centers, so you can confidently design AI-ready infrastructure that balances performance, scalability, and energy efficiency.


Connect with your local Motivair product specialist today.

TOP