Read more from DataCenter Dynamics on the launch of our Dynamic Cold Plates™.
Here's an excerpt:
The company's dynamic cold plates don't use skiving; they have grooves "wide enough to basically fit a penny in between them," Whitmore said, with the system able to handle particulates up to 400 microns. This means that the plate has a reduced surface area, "but we get the performance back by dynamically distributing the fluid across those grooves," Whitmore explained. "We do it uniformly across the entire cold plate - most of the technologies out there are entering in one side and coming out the other whereas we actually distribute from the top down, flowing the fluid across the entire surface area."