Cooling Solutions for Enterprise Data Centers at Industry Event

Motivair Corporation, based in Buffalo, New York, a global leader in mission critical cooling chillers for data centers and manufacturer of the ChilledDoor® Rack Cooling System, announces it will exhibit at DCD Enterprise, May 1 – 2, at the Marriott Marquis, Times Square, New York (Booth #105).

Read more about DCD Enterprise 2018 here.

At Motivair’s booth (#105), will be a complete demonstration of a ChilledDoor® Rack Cooling System, which is used to cool densities up to 75 kW per rack. The ChilledDoor® has been uniquely designed to eliminate “hot spots” in a data center by removing 100% of the server heat at its source for a fraction of the cost per kW. Using minimum fan power, it will “actively” respond to dynamic workloads assuring ultimate operator flexibility.  The door will also feature a custom graphic on the face of the ChilledDoor to showcase Motivair’s flexible design capabilities for OEM or end user applications to create a unique look throughout the data center.

For use in greenfield, co-location or retrofit data centers, today’s most advanced, high-efficiency data centers and computer systems are using ChilledDoor® technology as it requires little infrastructure change for initial operation and future growth. It offers a minimally invasive deployment (able to be used with any standard industry server rack, with or without raised flooring, no retrofitting replacement of servers required), which ultimately reduces overall costs – both upfront and when deploying additional compute.

Expo attendees will have the opportunity to learn more about other products and services designed to meet the needs of data centers, such as Motivair’s Coolant Distribution Units (CDUs) and maintenance and support services. In addition, information about Motivair’s free cooling chillers for enterprise data center or co-location applications will be available.  Free-cooling technology can provide data center owners and operators with unmatched efficiency and energy savings, especially in climates with considerably cooler winter months.  Click here to read a recent case study on Motivair’s chiller application for a large enterprise data center utilizing free cooling.

Representing Motivair at the event will be Regional Sales Directors Kevin Werely and Pete Peresie.

 

About the ChilledDoor® Rack Cooling System The ChilledDoor® Rack Cooling System, a product of Motivair Corporation, is a global leader in high efficiency and high density server rack cooling systems for small, medium and larger data centers. A trusted leader in developing advanced server cooling technologies, The ChilledDoor® Rack Cooling System, Coolant Distribution Unit and its ancillary support products and services provide innovative and dynamic new ways to cool both legacy and new data centers. Learn more at www.ChilledDoor.com.

About Motivair Corporation Motivair Corporation, based in Buffalo, NY (USA), is a globally recognized supplier of specialty chillers and cooling systems providing innovative solutions for customers in industrial, commercial, public and private sectors around the world. For more information, visit www.MotivairCorp.com.

 

Filed in the categories: News Release, Trade shows
See other innovative products! GO TO PRODUCTS